This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV3201-Q1 CFG and CURR Register (A-70)



Hello,

 

To check if CFG0-3 and CURR0-3 registers are not changed accidentally, MCU read these registers periodically and check if data are correct, and write correct data if read data in not correct.

 

But I want to write correct value for CFG0-3 and CURR0-3 registers periodically while controlling Motor instead of above operation to simplify the SPI sequence.

 

Please advise if there are any problem in case of CFG0-3 and CURR0-3 registers are written periodically while controlling Motor.

 

Best Regards.