Hi, All
I failed to activate 180 degree sin-wave driving on customer PCB with MSP430G2233+DRV8308+CSD18531.
I have set relative registers as below:
BASIC -> 0
ENSINE -> 1
MOD120 -> 3970
But still DRV8308 works as 120 degree driver.
Is there any other registers need to be set to particular value to activate sin-wave driving?
It worked with EVM, but I cannot access to soft codes built in MSP430 on the EVM.
It will also help if you could share the soft codes of the EVM for my reference.