This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8802-Q1, Low input voltage brushed DC driver

Guru 20090 points
Other Parts Discussed in Thread: DRV8802-Q1

Hello,

Are there the road map of motor driver which have the following specifications?

# of Full Bridges : over 2
Automotiver qualified
Operating Voltage range : 6V to 16V
Absolute maximum rating : over 32V
RMS output current : over 0.8A

I think that the DRV8802-Q1 is similar with this requirement but input voltage(min) of DRV8802-Q1 is 8V.

Best Regards,
Ryuji Asaka