Hello Team,
Could you please help us evaluating DRV10975 ? Our customer started evaluating the device with the EVM. When they applied power VCC=12 with motor connected, motor only span once a second. They had set JP2 to ANALOG-SP (Pin1-2), and POT to the maximum setting (around 3.3V).
Do you have any idea what is wrong with the procedure ? I believe DRV10975EVM could simply spin motor without using the GUI.
I have seen similar post in the following link. I have asked customer to try raising the VCC voltage up to 18V.
Best Regards,
Kawai