Other Parts Discussed in Thread: DRV2624EVM-MINI, DRV2624, DRV2624EVM-CT
I am using a DRV-USBCOM-EVM with a DRV2624EVM-Mini and the Haptics Control Console. Out of the box, this isn't running, so I am investigating the I2C communications. There's no literature on the DRV-USBCOM-EVM. From the writing on the PCB, I assume I have it hooked up correctly, but I'm not reading or writing registers. I see only two 7-bit address reads when I click "Connect." The console sees "0.TI-Haptics-MSP-USB2I2C v1.4".