This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8823 has ability to monitor the current/charge

Other Parts Discussed in Thread: DRV8823, DRV8806, DRV8846, DRV8881, DRV8848

1.We would like to connect DC latch Solenoid to DRV8823 and want to monitor if the solenoid switch its state by observing the current which is flowing through the DRV8823, is it possible?

If the answer is yes, how it is been done?

2.Are there cheaper alternatives for only 2 solenoids instead of 4 (which are supported in DRV8823)? (2 H-bridges)

3.What is the difference between DRV8806 and DRV8823? (Let’s assume that we need to hold 1.5A pulse and not 2A)

Thanks in advance