Other Parts Discussed in Thread: DRV8811, DRV8825
I've just designed a new circuit using the DRV8811 stepper motor controller and I'm having problems getting it to current limit.
I followed the current sense regulation instructions and used a 0.1872R resistor with a 3.0V reference voltage which should give me a maximum of 2A.It gave me a lot more current (I measured the voltage drop across the resistor with a scope) and I then dropped the resistor to 0.36R and I measured more than 600mV. I've also switched to a resistive load instead of a stepper motor (when I measured the 600mV).
It doesn't seem to matter what sense resistor I use, nothing seems to work. I've also noticed that one channel (bridge) seems to PWM/chop and the other channel just outputs a fixed voltage/current. With a very big sense resistor I got a few volts over it.
Any ideas / suggestions?
Thanks.