The datasheet says that the speed can be controlled by VCC and PWM input. So when should I use VCC and when to use PWM? Besides, do they have the same resolution? The datasheet only says: "The PWM input signal resolution is less than 1%"
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet says that the speed can be controlled by VCC and PWM input. So when should I use VCC and when to use PWM? Besides, do they have the same resolution? The datasheet only says: "The PWM input signal resolution is less than 1%"