Dear Motor Driver support team,
I control the driver on the DRV8880 Evaluation Module Board from the DSP on the C2000 Piccolo LaunchPad Evalution Kit Board.
The microstepping setting can be set by the two bits of M1 and M0 as shown in Table 1 on Page 15.
(I refer the manual: www.tij.co.jp/.../drv8880.pdf)
If I prefer to set the 1/8 or 1/16 step, I should set the MO bit to "Z". Is this "Z" mean high impedance?
I was wondering how can I assert "Z" from the DSP output?
I am looking forward your kind reply.
Yohjiro Kawai,