Dear Support team
I have one question regarding DRV10866
The datasheet has very little information about the maximal and minimal frequency.
In this forum, I have out, that the range might be from 18Hz up to 680Hz.
We are planning to use the DRV10866 at 100% PWM and 5.5V.
Is the a guaranty, that speed never exceeds 680Hz?
How constant is this speed? Does each DRV10866 behave a bit different?
The datasheet has just some typical values, see 6.6 Typical Characteristics of DRV10866.
At which power supply is this measured?
At which duty cycle is this measured?
What I also miss is the tolerance and the thermic dependence.
Best regards,
Rolf