Other Parts Discussed in Thread: , DRV10963
Using the DRV10866EVM (evaluation module board with motor provided in the kit) and a EZ MSP430 Launchpad (the USB dongle with separable target board.) I jumpered Vcc, Gnd, and a motorEnable signal between the boards. The MSP430 enables the signal for 0.1 second, then disable for 1 second. The signal from the MSP430 is taken from the same pin that drives the LED on the MSP430 eval board and drives the PWM pin of the DRV10866. Thus I am driving the motor full on for 0.1s, then full off for 1s.
->The motor responds say about ten times, and then quits responding. After spinning the motor’s shaft by hand, the motor resumes responding, for a while. When it does stop responding, it doesn’t seem to stop at any particular angle (at the resolution I can detect by eye, it could be it is always at an angle of a multiple of say exactly 90 degrees.)
I have powered the DRV10866 from the Launchpad’s USB driven power supply (5v?). In another trial I used a 2.8V battery. I also add a 1mF capacitor near the power pins of the EVM board (thinking the voltage was drooping and the driver entering under voltage lockout.) The battery leads are a few inches long.
I have tried removing jumper J2 (tying FGS to Vcc so that FG signal is 1/2 motor speed) with no change in symptoms.
I have waiting for more than 15 seconds, thinking it might be a false lockup detect that would expire, but motor never resumed responding.
While the motor is not responding, the FG test point seems to toggle low. I think this means the DRV10866 is trying to turn the motor (not in a locked up state.)
I see in another post a suggestion that the DRV10963 is a newer part. Is it a better choice for my application (just pulsing a motor very briefly say every ten seconds?)
I plan to try another smaller motor (the target motor is 3V, 10mm dia Maxon motor, but I don’t have one yet.) I plan to try other parameters, say ON a half second.
(Per Users Guide I have removed R6 to disconnect the DRV10866EVM PWM pin from the EVM’S 555 PWM signal. I don’t have an oscilloscope.)