This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8816: Max Current

Part Number: DRV8816


Hi there,

I'm considering using this component to drive two (different) solenoids, and i have a few questions:

1. Is the max current stated in the d.s is for each of the outputs (2.8A per 1/2 h bridge) or both of them?

2. i havn't seen any back EMF protection. Does it have any or should i place a diode to protect my circuit?

Thank you for your help!