DRV8872Q1 met issue in one automotive account.
Attached motor structure and parameter.
All the test were run on EVM.
If set INx prior to VM, the motor can start-up and spin.
If set VM prior to INx, the nFault indicator LED lights on, waveform shows OCP seems to be triggered and auto-restart every 3ms.
Replaced current sensing resistor to 150mohm, 330mohm, 400mohm, 500mohm, 750mohm, 1ohm. The issue remains.
Considering the charging to capacitor leads to the OCP during start-up at high VM, current limitation should help to limit the start-up current and get the motor spin.
Wonder why the current regulation circuit seems does not effective in this case.