Other Parts Discussed in Thread: TPL7407L, DRV8805, , DRV8833C, DRV8839
Hi,
I need to run the 28 BYJ-48 stepper motor in unipolar mode with a supply voltage of 5V. This stepper is usually driven with ULN2003. However, the ULN2003 may not be the most efficient driver due to high saturation voltage. I wonder if there are more efficient choices.
Again, the stepper will be powered using 5V, and the maximum current through each coil is roughly 200mA, so each channel of the driver must be able to handle that.
I looked at the TPL7407L, which is essentially a NMOS version of the ULN2003, but it requires a COM voltage of at least 8.5V.
I looked at the DRV8805, but that also requires a 8.2V supply voltage.
I'm also considering the DRV777, however, the maximum current per channel is only 160mA. (I heard it can be paralleled for more output?)
The driver will be controlled from a microprocessor with 5V signal.
I hope you can make a suggestion on driver choice. Efficiency is important since I want to commercialize the design.
Thanks