Hi,
Customer thinks to use DRV8880.
Condition is full step and 20mA full scale current.
Is it possible?
DRV8880 operates the current setting value 71% with full step.
For the reason, I think that 30mA full scale current setting is better.
The concern is accuracy of the current limit detection.
I think that the accuracy is bad from Figure 10.
If it is possible on specification, I tell customer to try at EVM.
Best regards,
Shimizu