Hello TI Support.
I have a DRV8711 and stepper motor 24HS39-3008D (BIPOLAR configuration where torque is 4.0Nm and inductance 3.0mH/1kHz). Power supply is 36V or 48V.
DRV8711 shall works with 1/32 microsteps and up to 200kHz steps frequency.
I am testing this driver using DRV8711EVM and external steps/dir generator to obtain good acceleration (from 1kHz to 200kHz).
I have a problem with settings because I can obtain only 60kHz and motor stops. What is the correct settings?
Now I have settings like on attachment.24HS39-3008D.pdf