Other Parts Discussed in Thread: TIDA-00875,
Hi,
One of my customer designed a single phase BLDC operated on 12V using DRV8801 with reference from TIDA-00875.
1. When i try to stop the fan blades physically using some obstacle like screw driver or pencil, the motor stops, and then starts moving again after I remove the obstacle, which is good. But there is no any indication on nFAULT pin in this case, nFAULT remains HIGH. Can this condition be detected using nFAULT?
2. Customer wanted to increase the RPM for the same blades connected to the motor. Please suggest on this.