This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8839EVM: Question of the DRV8839DSGR's Operation Voltage Range

Part Number: DRV8839EVM
Other Parts Discussed in Thread: DRV8839

Hi Sirs,

Would you please advise that if we can use 5V VM and 1.8V VCC, while the test conditions on the datasheet is 3.3V VCC?



Thank you and Best regards,

Wayne Chen
12/22/2017