What is the recommend minimal configuration for a 12V 0.5A BLDC Fan Motor that with variable speed control and the possibility to change rotation direction.
Can this be achieved without direct MCU control for example with PWM input to the DRV. For example duty < 50% = cw , duty>50% = ccw.
I would prefer a sensor-less design because of the ease of the motor.
If MCU is needed, please suggest a configuration and design example.
Production will be about 10k unit per year. (no over-spec. suggestions please. )
Do you have motor control examples for CC1350? If possible I want to control the motor directly via Sub-Giga band.