This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8812: The output is absent

Part Number: DRV8812
Other Parts Discussed in Thread: DRV8412

Hi to all, I'm using this driver to drive a DC motor.

I shorted to gorund M!, M2 and M3. I powered the IC with +12Vdc and I provided a complementary PWM at the input (PWM_A and PWM_B) but the OUT_A and OUT_B are also 0V.

I checked that the RESET pin are high and there are no fault.

What an I wrong?