Part Number: UC2625
Hello,
I am using the UC2625 and I cannot seem to pinpoint which block will the turn-off and turn-on threshold directly affect, and does PWR VCC and VCC have to be supplied with the same voltage?
Thank You
Youssef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UC2625
Hello,
I am using the UC2625 and I cannot seem to pinpoint which block will the turn-off and turn-on threshold directly affect, and does PWR VCC and VCC have to be supplied with the same voltage?
Thank You
Youssef
Youssef,
VCC below 9V will tr-state driver.
What type of output stage did you use for driving low side? Are you suing Darlingtons or NPETs?
Thanks
Seil