This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605L-Q1: Waveform content of each library

Part Number: DRV2605L-Q1


Please can you confirm that each of the selectable libraries: 5 x ERM and 1 x LRA contains or includes all 123 possible waveforms? i.e. the library selection limits certain parameters but contains all 123 waveform options.

  • Hi Paul,

    Each library contains 123 effects, so you can use the index from 1 to 123 in the waveform sequencer. There are 6 x ERM and 1 x LRA (total 7).
    The differences between the ERM libraries are listed in data sheet table 1 (page 14).

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators