Other Parts Discussed in Thread: DRV8703-Q1, DRV8704, DRV8702-Q1, DRV8800, DRV104, DRV103, DRV8871, DRV8870, DRV8872
Hi,
There are two half-bridge in DRV8816 chip, I want to tie the EN1 and EN2 together (also tie IN1 and IN2, OUT1 and OUT2) so that it can provide double drive current, is it possible to use the chip in this way? I worry if there is difference in the propagation delay or internal dead time between two half bridge.
Thanks.