Other Parts Discussed in Thread: CSD
Hello,
Could you tell us about CSD 88539?
What is the avalanche (EAR) value under the following conditions?
※ This question is about EAR, not EAS.
VDD = 30 V,
Vgs = 20 V -> 0 V,
ID = 10 A,
L = 100 uH,
RG = 25 ohms
Tch ≦ 150 ° C., test time 1000 h
On = 1 us, duty cycle ≦ 1%
Thank you.