Flyback Transformer Datasheet Discrepancy
Hello,
I am working on a BLDC motor driver using the DRV10983. In the application note it refers to a transformer that is used in the AC-DC to generate 24VDC from AC mains input. Here is the datasheet of the transformer.
http://www.ti.com/lit/ug/tidu354/tidu354.pdf
We are building that transformer right now but we have noticed a discrepancy between the bobbin datasheet and the photograph of the assembled transformer.
Please compare Page 2 and Page 3 in the datasheet.
Can someone please throw light on this or if there is a corrected datasheet that will help too.
Thanks and Regards
Ajay