Hi
1.
LDO function of DRV8850 is not used in the application.
Could you please tell us adequate termination of LDOEN, LDOFB and LDOOUT?
To saving power, could they be left open?
2.
We will need only forward driving.
Is the following connection correct?
IN1H : PWM
IN1L : ~PWM
IN2H : GND (with 1Kohm)
IN2L : VCC_3.3V (with 1Kohm)
3.
Can we use SR resistor by 2.4Kohm?
BestRegards