This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8704: DRV8704-EVM

Part Number: DRV8704
Other Parts Discussed in Thread: TMS320F28379D, BOOST-DRV8711,

Hello

·        Can we connect DRV8704 Evaluation Module to Delfino TMS320F28379D LaunchPad?

·        What is the maximum volt that can be applied to the motor using DRV8704 Evaluation Module? The DRV8704 Evaluation Module manual does not seem to state that.

·        What is the maximum continuous current that can be applied to the motor using DRV8704 Evaluation Module? The DRV8704 Evaluation Module manual does not seem to state that.

Regards

Sam

  • Hi Sam,

    (1)· Can we connect DRV8704 Evaluation Module to Delfino TMS320F28379D LaunchPad?

    >> The DRV8704EVM was tested with the MSP-EXP430G2 LaunchPad. The BOOST-DRV8711 is a similar EVM. Using the BoosterPack compatibility ( dev.ti.com/.../ ) shows the Delfino TMS320F28379D LaunchPad should work, but has not been confirmed.

    (2)· What is the maximum volt that can be applied to the motor using DRV8704 Evaluation Module? The DRV8704 Evaluation Module manual does not seem to state that.

    >> The DRV8704 was designed to operate across the recommended operating voltage range.

    (3)· What is the maximum continuous current that can be applied to the motor using DRV8704 Evaluation Module? The DRV8704 Evaluation Module manual does not seem to state that.

    >> Maximum continuous current is approximately 10A.