I have a drv8301-hc-evm rev d kit and a scheme.
I used to run 48V BLDC Motor.
Under the motor max current, I know that kit's R107, R95; R108, R105; R113, R103 must be changed because of Rfb = [(3.3V-1.65V)(Max current*0.002)]*Rin.
So, do we have to change Rfb resister(R107, R95; R108, R105; R113, R103) every time the motor?
Or when motor change, motor's max current is changed.
Q1. could I use kit without Rfb value change?
Q2. What is voltage filter pole? Is it like LPF?