This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2511-Q1: Question about input common mode voltage

Part Number: DRV2511-Q1
Other Parts Discussed in Thread: DRV2510-Q1

Hi Champs,

 I got below questions from customer, could you support these?

 Q.1) VICMIN and VICMAX are the same spec as DRV2510-Q1?

 Q.2) With the circuit configuration as figure 10 of datasheet and Gain = 20dB(10V/V), if IN+ and IN- supplied as shown I attached file, can we expect same output signal on OUT+ - OUT- with 6Vpp pulse?

 Q.3) In above cases, will the duty of the pulse affect to common mode input level?

For example, if high pulse duty is narrow as shown in Fig.3, can we think common mode input level is still 0.3V?

Best regards,

Nobuo FujiharaINPUT signal.xlsx