Hi Team,
We are designing DRV3245 PCB
Can I Use 0Ω resistance at current measure input route ?
Can we change CSA output filter parameter from 1K/1nF to 330R/470pF?
Can we choose 25V cap for CP1 and 50V cap for CP2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
We are designing DRV3245 PCB
Can I Use 0Ω resistance at current measure input route ?
Can we change CSA output filter parameter from 1K/1nF to 330R/470pF?
Can we choose 25V cap for CP1 and 50V cap for CP2?
1. Can I Use 0Ω resistance at current measure input route ?
Ans 1 : Yes, you can use 0Ohm.
2. Can we change CSA output filter parameter from 1K/1nF to 330R/470pF?
Ans 2 : Yes
Can we choose 25V cap for CP1 and 50V cap for CP2?
Ans 3 : CP1 and CP2 cap ratings are based on PVDD voltage. CP1 will see the full PVDD voltage and CP2 will see (PVDDx2)
If the PVDD voltage can be controlled ( unlikely for automotive load dump) , then the capacitors may be derated.