Other Parts Discussed in Thread: TPS92518, TPS54286, , TPS54283, TINA-TI
I need a SPI-controlled buck-regulator with an output ranging from 12V to 24V with 0.5V step resolution. The input voltage is 28V and the max load is 1.5A. I also need a second buck regulator with a fixed 7VDC output with a max load of 0.5A. Will the DRV8806PWPR do the trick ? If not, what solution would you recommend ?