Other Parts Discussed in Thread: , TMS320F28027F
Dear ALL
Pls help suggest to me , Customer is need to know Input current wavefom of DRV8305-Q1EVM .
Thank you so much & Bestregard
Prarinya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear ALL
Pls help suggest to me , Customer is need to know Input current wavefom of DRV8305-Q1EVM .
Thank you so much & Bestregard
Prarinya
Hi Prarinya,
Section 8.1 of the datasheet only says the following:
"The DRV8305-Q1 is a gate driver IC designed to drive a 3-phase BLDC motor in combination with exeternal power MOSFETs. The device provides a high level of integration with three half-bridge gate drivers, three current shunt amplifiers, adjustable slew rate control, logic LDO, and a suite of protection features."
I see nothing mention of any "signal test" in this section. Are you referring to the Application Curves in section 8.2.3?
The DRV8305-Q1EVM features an on-board TMS320F28027F microcontroller to provide the control and input signals for the DRV8305-Q1. The user's guide contains instructions for how to set up the hardware and install the GUI for controlling the EVM. When set up per these instructions, the GUI will program and control the on-board microcontroller, which will provide the necessary input signals for the DRV8305-Q1 to drive the output stage and spin a BLDC motor.
Thanks,
Garrett