As per the calculation for Output Inductor Selection:
PVDD=50 V
Toc_delay = 250 ns (as given in the datasheet)
Ipeak = 15(as given in the datasheet)
Iavg=8 A.
L=1.785 uH for 13A.
I have selected 1.5uH and 20.5A inductor. But it is large in size.
As per my space requirements I can go for smaller size in Inductor.
Please suggest.