This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625: DRV2625 Auto Calibration and Diagnostics Process Failled Both

Part Number: DRV2625


Hey,

I am Evaluating DRV2625EVM-MINI Evaluation Board with an Linear Resonant Actuator whish spécification are:

-Vibration-Frecency: 2.5Grms@100Hz(Fact)

-Thermal Resistance: 15.3Ω

-Power Consumption: <300mW @2.23Vrms(Sine Wave)

-Response Time <30ms

Following this Specifications, i have to set Drive Time to 1/(2*Fact)=5ms (see DRV2625 Datasheet at Page 23). But DRIVE_TIME Registor can hold a maximum Drive Time of 3.6ms (see page 54)

I also Have to Set RATE_Voltage register to 0x64 Value as motor Rate voltage is 2.23Vrms. The Clamp Voltage is 2.23*sqr(2)<3.16V so I have to set CLAMP_VOLTAGE register to 0x95 Value.

Please see attached Data for other value that i use for other configuration registers.

Now, when i run Calibration Process (1000ms), the process failled with none Over-current, Over-Temperature or under Voltage detection. The Diagnostics Process also failled with None Error detection.

Am I done something Wrong? How can i Fixed these issues?

Thanks.

DRV2625 Process.pdf

  • Part Number: DRV2625

    Hey,

    I am evaluating, the DRV2625EVM-MINI Evaluattion borad  with an Linear Resonance Actuator whish specification are:

    -Vibration Frequency: 2.5Grms@100Hz (Fact)

    - Rated Voltage,2.23Vrms

    -Response time <30ms

    -power consumption <300mw@2.23Vrms (Sine Wave)

    Following these specifications, i have to set Drive Time to 1/(2*Fact)=5ms (see DRV2625 Data sheet at page 23). But the maximum Drive Time Allow in DRIVE_TIME Register for LRA actuator is 3.6ms (see Page 54)

    to Get a Rated Votage of 2.23Vrms, I have to set RATE_VOLTAGE register to 0x64 value. The Clamp Voltage is 2.23*sqr(2) < 3.16V so i have to set CLAMP Voltage to 0x95value.

    Please See attached File for other Value Configuration register that i used.

    Now, when i do Calibration (1000ms) it failed with none over-current Dection, over-temperature or Udervoltage detection. Diagnostic Process Failed with none Error Detection.

    Am I do something Wrong?

    How can i resolve this issue?

    Thanks

    Th

  • Hi Jean,

    We'll check your issue description, but in the meantime: Is your actuator attached to a mass during Calibration/Diagnostics?
    If the actuator is not fixed to a mass, the vibration feedback might no be correct.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hey Ivan,

    Thanks for your reply,

    Actually, The Actuator is not attached tu a mass. i'll try with an attached Mass.

    Thanks.

  • Jean,

    Please let us know how this test goes.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

  • Hi Jean,

    Did you got a chance to test the device with a mass attached to the actuator?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators