Hi,
We need to drive a DC motor through an I2C interface. The DRV8830 fits very well, except that max current in our DC motor must be limited to 92mA.
In DRV8830 datasheet, Current limit sense voltage VILIM is 200mV typical and Current limit sense resistance RISEN must be less than 1 ohm (§7.3.3). As a consequence, it seams to be impossible to set a current limit less than 200mV/1ohm = 200mA.
Could you explain why sense resistance must be limited to 1 ohm ? What is the issue if a 2.2ohms is used to limit current to 200mV/2.2ohms = 91mA ?
If not possible, do you have an application circuit using a resistance less than 1ohm and still limiting current below 200mA ?
Thanks in advance
David FREON