Hi,
I see from the datasheet that nominal PVDD is 50V. I also see an example application with PVDD of 24V. Finally, table 7.2 show a minimum of 0V on PVDD.
In my application (coil driver) in need to use 5V or lower.
I just want to confirm if the DRV8332 can reliably operate the output stage with 5V PVDD (or even lower) ?
Does this affect the maximum PWM frequency that can be used?
Thank you very much