Other Parts Discussed in Thread: DRV8872-Q1
Hello supporting team,
Could you tell me why duty cycle range of DRV8872EVM is different from that of DRV8872-Q1?
I saw [It is capable of an approximately 25-kHz output that can be adjusted from 5% to
95% duty cycle. This square output signal will switch from 0 V to V5P0.] in datasheet of DRV8872EVM
On the other hand, datasheet of DRV8872-Q1 says [The IN1 and IN2 pins can be set high and low for 100% duty cycle drive, and ITRIP can be used to control the
current, speed, and torque capability of the motor].
DRV8872EVM could not operate when duty cycle is <5% or >95%, is it correct?
Best regards,
Ochi