Other Parts Discussed in Thread: DRV8305
Dear All:
The DRV8305 datasheet have the specification of PVDD-VDRAIN 10V ~ -10V. But the DRV8305-Q1 datasheet didn't list it.
Is the DRV8305-Q1 has no limitation on PVDD-VDRAIN?
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All:
The DRV8305 datasheet have the specification of PVDD-VDRAIN 10V ~ -10V. But the DRV8305-Q1 datasheet didn't list it.
Is the DRV8305-Q1 has no limitation on PVDD-VDRAIN?
Andrew
Andrew,
Let me check and get back to you later today.
Regards,
-Adam
Andrew,
Could you explain your reasoning for needing this spec? What phenomenon are you safeguarding against?
Regards,
-Adam
Hi Adam
We are using drv8305q1 to design bldc control. In our design,the PVDD and VDRIAN pin is difference source same voltage 24V. when motor go to generator mode, drv8305 is damaged. So,We connect PVDD and VDRAIN pin source together. But Still have a chance to break the DRV8305. We are finding the root cause.
Andrew,
Did you review this section in the DRV8305-Q1 datasheet: 9.1 Power Supply Consideration in Generator Mode
Regards,
-Adam
Hi Adam,
We have one condition to make PVDD=24V,
VDRAIN(Pin44) connect to 100ohm pin1 and 100 ohm pin2 short to 0V in a very short time (we use 2 different power sources, one power for PVDD, another power for VDRAIN and motor MOSFET power)
And we find DRV8305-Q1 PVDD is short to ground , and dead forever in this condition.
We'd like to know if [DRV8305-Q1] DRV8305NQPHPRQ1 has the same "Voltage difference between supply and VDRAIN(PVDD-VDRAIN) +/-10V" spec as "DRV8305",
and check if this is the damage root cause,
Because we can not find this statement in "DRV8305-Q1" datasheet , but in "DRV8305" datasheet, thanks
BR,
Joseph
Joseph,
I don't understand your experiment: "VDRAIN(Pin44) connect to 100ohm pin1 and 100 ohm pin2 short to 0V in a very short time (we use 2 different power sources, one power for PVDD, another power for VDRAIN and motor MOSFET power)"
This should be the same spec yes.
Regards,
-Adam
Hi Adam,
Thank for your information, just double confirm:
In conclusion, DRV8305-Q1 and DRV8305 both need to follow
"-10V < (Voltage difference between supply and VDRAIN(PVDD-VDRAIN)) <10V".
Otherwise, driver ic may damage.
It means we can not use PVDD=24V and let VDRAIN=0V, right?
BR,
Joseph