Other Parts Discussed in Thread: DRV8350, DRV8353, DRV8350R, DRV8353R
Hi,
I'm designing a H-bridge controller for a brushed DC motor (48V @ 30A) and I decided to use the DRV8704. I don't know if there's any full bridge controller that fits better for this application (or maybe two half-bridges synced, I don't know).
The matter is that I don't need the current limiting of the DRV8704 and I want to simplify the PCB as much as possible. In the datasheet of the DRV8701 says that:
"This shunt amplifier feature can be disabled by tying the SP and SN pins to GND. When the amplifier is disabled, current regulation is also disabled."
But I don't know if I could do the same in the DRV8704. Also, I want to drive only one H-bridge so I don't know if there will be any other problem with my design.
Summing up:
- Is there a better solution for driving a brushed DC motor at 48V / 30A with external N-channel MOSFETs? I also want to have 100% duty cycle available.
- Could I remove Rsense and tie the current sense pins to ground?
- Could I use the DRV8704 with only one H bridge?
Thank you.