Other Parts Discussed in Thread: DRV8353R, DRV8353, DRV8353RS-EVM
Hello team,
at one of my customers, they are planning to develop a motor control application where the motor works with a 48V rail, nominal current of 13A and a frequency of 16-20KHz.
At first I was thinking of the DRV8332 but it has a nominal current of only 8A so it would be working on peak current all the time. Do you have any better suggestion/ recommendation?
Also, could you please recommend any MOS to be added to the gate driver? Due to the high current, the idea is to use 6 discrete mosfets and 3 Rsense.
Please let me know our ideas/suggestions.
Thank you in advance.
Best regards,
Adrian