Other Parts Discussed in Thread: DRV8711EVM
Hello,
There is conflicting message on datasheet of the DRV8704 about the SCS PIN which I have highlighted on the attached picture.
When sending a SPI command/ message does the SCS PIN need to be HIGH or LOW?
From the diagram it seems to be high but the text says:
"To complete the read or write transaction, SCS must be set to a logic 0."
Is there any example code that shows SPI read operations for DRV8704 for Code Composer ?
Thanks,
Mikias Mekonnen