This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: DRV8711DPC FAULT PIN ENABLE

Part Number: DRV8711
Other Parts Discussed in Thread: CSD88537ND, CSD88539ND

Dear Sir,

               I am using DRV8711 to drive 4 motors on one PCB. When we do run-in mode before functional test. The fault pin active sometimes. We tried to adjustment the software and different PCB layout. But the situation still happens. Can someone help to solve this problem? Many thanks.

Jason  

  • Hi,

    Have you tried reading the SPI registers to see what type of fault is occurring? 

    Do you think you can share with me your schematic?

  • Hi,

         The register shows over current error. Below are the schematics. DRV8711 DRIVER REV3.pdfDRV8711 DRIVER REV4.pdf

  • Hi,

    Thank you for sending the schematic. I have a couple questions.

    • Are you seeing the OCP fault being triggered on all four IC's or just on certain ones?
    • Can you send me your SPI register settings?

  • Hi,

         All 4 motors occurs fault signal. Motor1>>5%, Motor2>>10 %, Motor3>>25%, Motor4>>>60%. Below are the motor spec:

    Motor 1: 2.4VDC, 2A/PHASE, 1.2ohm

    Motor2,3,4:2.6VDC, 4A/PHASE, 0.65ohm, 2.4mH

    CTRL Resister: 0x0C34

    TORQUE Resister: 0x07FF

    OFF Resister: 0x0030

    BLANK Resister: 0x00FF

    Decay Resister: 0x0410

    STALL Resister: 0x0040

     DRIVE Resister: 0x006A

    Regards

    Jason

  • Hi Jason,

    Pablo is not available today, so I am responding for him. Thank you for the additional information.

    There are a few register settings to address.

    First, please change the DECAY register to either 0x0510 (auto mixed decay) or 0x0310 (mixed decay) as a starting point.

    Then please change the BLANK register to 0x0180 (adaptive blanking and 2us TBLANK)

    The TORQUE register should be set to either 0x075D (.05Ohm resistor) or 0x0782 (.07 Ohm resistor). This should limit the current to 4A full scale

    These changes should help get you closer to your goal and hopefully remove the overcurrent faults. The overcurrent faults were probably due to a combination of setting the TBLANK too long and the TOFF too short.

    For more information, please see the Decay Mode Setting Optimization  and DRV8711 Quick Spin and Tuning Guide www.ti.com/.../SLVA632

  • Hi  Rick,

                   Thank you for your reply. I will let our engineer to do more test when change the register. And we also notice a interesting thing. We change the MOSFET CSD88539ND to CSD88537ND. Suddenly the issue are solved without adjusting the register setting. Do you think any possibility the issue comes  from the MOSFET? And do TI have the recommended MOSFET list or how can we to select a suitable one? Thank you for your support.

    Jason

  • Hi Jason,

    Changing to the lower Rdson FET reduces the VDS voltage, and is probably masking the OCP error.

    But the OCP threshold is set at 750mV, which equates to ~32A  (750mV/23mOhm) through the FETs. This is too much current and needs to be addressed.

    If you have a current probe you will probably see this large current for a short period of time.

  • Hi Rick,

                 We tried to adjust the register you told us. But it's the same result. Is there any other solution?

    Regards

    Jason 

  • Hi Jason,

    Do you have a current probe? If so, please provide a scope capture of the current through the windings just prior to the nFAULT signal asserting.

    This will help provide information on the cause.

    If you do not have a current probe, please provide a scope capture of the voltage across the sense resistor to GND prior to nFAULT asserting. This can be more difficult to interpret.

    Has the firmware engineer confirmed the registers writes?

    If the motor is not connected, do you get the OCP fault? If so, please check the layout.

  • Hi Jason,

    Do you have any updates?

  • Hi Jason,

    If you still have problem there are some my suggestions

    1. Use gate resistor (47 - 100 Ohm) for low side MOSFETS

    2. Try to eliminate RC filters for AISENN/AISENP (differential pair from sense resistor to AISENN/AISENP placed over PCB ground layer could be sufficient) 

    Less important:

    3. Instead of polymer caps decoupling 24V, better choice might be 10-100nF MLCC for each high side MOSFET (placed as close as possible to these mosfets and GND) + 1uF- 2,2uF MLCC for each

    H-bridge + single 1000uF - 4700 uF electrolytic cap to store energy from vibrations and breaking.

    4. Use 4 layer PCB with 1-2 ground layers if possible.

    5. 0,022 - 0,033 Ohm resistor might be a better choice for 4A (less power losses and still good current control)

    Grzegorz

  • Hi Jason,

    Do you have a current probe? If so, please provide a scope capture of the current through the windings just prior to the nFAULT signal asserting.

    This will help provide information on the cause.

    If you do not have a current probe, please provide a scope capture of the voltage across the sense resistor to GND prior to nFAULT asserting. This can be more difficult to interpret.


    Thank you for the scope captures. Can you answer a few questions about them?

    1) What is the scale in the current captures? 10mV = ?A
    2) Is the motor accelerating (STEP frequency increasing) in the PHASE A and PHASE B image?
            What is the STEP frequency range?
    3) When did the fault occur in 2. Motor Current Waveform (Fault pin enabled)
    4) What fault was reported by the DRV8711?
    5) What is the STEP frequency in Image 1 of the shunt resistor images?

     

    Has the firmware engineer confirmed the registers writes?

    If the motor is not connected, do you get the OCP fault? If so, please check the layout.

  • Hi Rick,

                 I need more time to do test. Will update later. Thank you for your support.

    Jason

  • Hi Jason,

    Thank you for the update. For now we will close the thread.

    Please reply to it when you have an update. If the thread is locked, please select "Ask a related question" at the top of the thread.