This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: Full bridge configuration

Part Number: DRV8844

Connected the dev board DRV8844EVM to my control outputs; 2 direction lines and one PWM output.

I connected output 1 and 2 on one side of the motor and output 3 and 4 on the other side.

I then connected the control pins based on the Table 2 in the data sheet for fast decay.

Connected IN1 and IN2 to one control line, connected IN3 and IN4 to other control line and connected the PWM to EN1, EN2, EN3 and EN4.

There is PWM output but not motor movement. So I am assuming I have the bridge or pin configuration incorrect.

Please let me know the best setup for a single DC motor.

Thanks - Matt