This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: ground isolation

Part Number: DRV8844

Hi,

I was wondering if the logic ground pin (LGND) is electrically isolated from VNEG and PPAD? I'd like to use separate grounds for the microcontroller and the motor, and am wondering if I can connect LGND to my 'clean' ground and VNEG/PPAD to the motor ground?

If so, I'd like to confirm which pins are referenced to LGND; is it all the INx / ENx, nRST, nSLEEP, and nFAULT?

thanks,

Ryan