Other Parts Discussed in Thread: DRV8802
Hello Everyone,
We have developed working prototype using DRV8802 motor driver IC, after developing custom PCB we are facing some issues. We have compared voltage values on all the pins(on DRV8802) in prototype board and custom board and we see following differences
Pin Description | Voltage on prototype Board | Voltage on custom borad |
VCP1 (Pin 1) | 5.7V | 1.78V |
VCP2 | 18.26V | 10.68V |
VCP | 25.34V | 0-2.0V |
The above values are taken at 13.5V supply voltage and the motors are not operating in the custom board whereas it is working in prototype board.
Request to help us in debugging this issue.
Regards
Brijender