Other Parts Discussed in Thread: MSP-EXP430F5529LP, MSP430F5529, DRV8320
Hi All,
I need help to know if with the combination of the MSP-EXP430F5529LP + BOOSTXL-DRV8320 controller to spin a BLDC motor, it could work with the following features:
* Voltage rated 24 Vdc.
* Current rated 10 Amp.
* Close loop control (Hall Sensors).
* Speed control external or internal (no relevant).
* If the speed increases up to seting for external conditions, actived brake to reduced at set point.
Is there any software to be able to see the motor variables speed, torque, current ...?
Would the DRV8312 Evaluation Kit be better?
Suggestions?
Thanks in advance!