Hello Team,
My customer is planning to use DRV10983-Q1 with regulator in linear mode. The do not have any external load to be powered from DRV10983-Q1.
Can they use 0.2W rated resistor instead of 1/4W?
Continuous max VCC voltage is 24V and transient is 38V
Recommended value for linear regulator in datasheet is 39ohm. can we use 47ohm or 50ohm here?
Regards,
Mahendra