Other Parts Discussed in Thread: USB2ANY, , DRV2625
Is there any way to work with this board in Windows 10?
Kind regards,
Jorge Elizalde
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any way to work with this board in Windows 10?
Kind regards,
Jorge Elizalde
Hi, Jorge,
Welcome to E2E and thank you for your interest in our products!
Do you have the USB2ANY tool? When working on Windows 10, this EVM requires of this additional device to fully control the board.
Please let me know if you have questions or comments on this. We will be glad to help you.
Best regards,
Luis Fernando Rodríguez S.
Hi Luis,
I only have the DRV2625EVM-CT evaluation module.
So, do I need to by the USB2ANY interface adapter? https://www.ti.com/tool/USB2ANY
In this case, is it enough? I mean, if I need anything else, please tell me, to buy everything at the same time.
Kind regards,
Jorge
Hi, Jorge,
Yes, this would be the only tool that you will require to have the EVM fully operating.
Best regards,
Luis Fernando Rodríguez S.
Hi,
Regarding the DRV2625EVM-CT evaluation module, where should the ribbon cable be connected? The ribbon cable is provided?
Thanks,
Jorge
Hi, Jorge,
You would just require of three pins to connect the USB2ANY to the DRV2625EVM-CT:
- SCL.
- SDA.
- GND.
You can use single female-to-female wires to connect these pins to J4 pins connector.
Best regards,
Luis Fernando Rodríguez S.
Hi,
I have the USB2ANY kit.
I found the instructions on the Haptic Control Console GUI User's Guide
Thanks
Jorge
Hi, Jorge,
Were you able to use the Haptics Control Console with the USB2ANY tool? Please let me know if you require additional support from our side.
Best regards,
Luis Fernando Rodríguez S.
Hi,
I've been able to connect with the USB2ANY using HCC, but when I choose the console tool for the DRV2625, I still continue viewing: "Console : DRV2625 -- Simulator".
I'll try again after rebooting the whole system.
We'll be in contact!
Thanks,
Jorge
Hi Luis,
I cannot connect. Perhaps the order it's not correct. I've followed the steps:
But I obtain "Console : DRV2625 -- Simulator" instead of USB
Jorge
Hi again,
The window title says "Simulator", but I tried.
If I press START in Work Mode the LRA works.
But the software is a little bit tricky...
Kind regards,
Jorge
Hi, Jorge,
Could you try with these steps, please?
1.- Connect DRV2625EVM-CT to USB2ANY.
2.- Connect USB2ANY to computer.
3.- Press the + button for GUI mode (F is seen in the LED's display).
4.- Open HCC
5.- In HCC: USB 0.Haptics DRV-USBCOM-EVM v1.4 -> CONNECT
Best regards,
Luis Fernando Rodríguez S.
Hi,
It works...but only with the integrated LRA. The integrated ERM actuator doesn't vibrate in this GUI mode. I tried a lot of parameters but I cannot. And this ERM works perfectly with the pre-programmed effects.
I connected an external ERM to the OUT and it also works.
Thanks,
Jorge