This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10974: 12poles BLDC motor

Part Number: DRV10974

Hi team,

My customer is interested in the DRV10974. Is it possible to use the DRV10974 to 12poles BLDC motor?

Regards,

Yamaguchi

  • Hi Takashi,

    Thanks for posting your question in MD forum. We can't really decide if DRV10974 can be used just based on Motor pole pairs. Choosing DRV10974 actually depends on several motor parameters. Please check the recommended application range table below. Compare this with the motor datasheet and if the values fall within the recommended application range then DRV10974 can drive your motor. 

    Regards,

    Vishnu