Hi Expert,
I want to confirm about the following datasheet description.
Note that if the step mode is changed from full, 1/2, 1/4, 1/8, or 1/16 to full, 1/2, 1/4, 1/8, or 1/16 while stepping,
the indexer will advance to the next valid state for the new MODE setting at the rising edge of STEP.
If customer will change from Full step to 1/2 step while stepping, which is correct?
Blue : the indexer will advance with new mode(1/2 step) by next step signal
Green : the step mode will change to new mode by next step signal
Thanks
Muk